SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
Each proxy thread must have a single owner, as each proxy thread only has a single buffer to work on the current data. If there are multiple owners in the system, they must each use their own proxy thread. Then they will have their own buffer and each can access a different resource at the same time. Each proxy thread is completely independent and kept coherent regardless of accesses to other proxy threads or regardless of the order of accesses. So the proxy support interleaving of multiple hosts' accesses.