SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The CSI_RX_IF will detect the error condition and capture the associated VC, DT and WC information for the packet header before generating an error interrupt flag on CSI_RX_IF_VBUS2APB_ERROR_IRQS.
The CSI_RX_IF will continue processing the current frame and continue the stream when a header Reserved DT or a long packet payload CRC error is detected.
The CSI_RX_IF will stop processing the current frame and continue the stream when a packet header ECC error is detected, as the current frame synchronisation cannot be maintained.