SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
The Power-AP has a DEBUGATTENTION directive that is used to indicate the execution state of a CPU or other debugable module in the managed domain, without having to establish a direct debug connection to that CPU. When the associated CPU is halted by debug, this directive is asserted. Tools can read that in the Power-AP. Since halted cores generally prevent power transitions in their domains, the tools can be assured that they can safely connect to the debug logic in the CPU.