SLAU132V October   2004  – February 2020

 

  1.   1
    1.     2
    2.     3
    3.     4
    4.     5
    5.     6
  2.   7
    1.     8
    2.     9
    3.     10
    4.     11
    5.     12
  3.   13
    1.     14
    2.     15
    3.     16
      1.      17
      2.      18
      3.      19
      4.      20
      5.      21
      6.      22
      7.      23
      8.      24
      9.      25
      10.      26
      11.      27
      12.      28
    4.     29
      1.      30
      2.      31
    5.     32
      1.      33
      2.      34
        1.       35
      3.      36
      4.      37
      5.      38
      6.      39
      7.      40
      8.      41
      9.      42
      10.      43
    6.     44
    7.     45
      1.      46
      2.      47
    8.     48
    9.     49
    10.     50
    11.     51
      1.      52
      2.      53
    12.     54
      1.      55
    13.     56
    14.     57
  4.   58
    1.     59
    2.     60
    3.     61
      1.      62
    4.     63
      1.      64
      2.      65
    5.     66
    6.     67
      1.      68
      2.      69
    7.     70
      1.      71
        1.       72
        2.       73
        3.       74
        4.       75
        5.       76
        6.       77
        7.       78
        8.       79
      2.      80
      3.      81
      4.      82
    8.     83
      1.      84
        1.       85
        2.       86
      2.      87
        1.       88
        2.       89
        3.       90
    9.     91
    10.     92
    11.     93
      1.      94
      2.      95
    12.     96
    13.     97
      1.      98
      2.      99
      3.      100
      4.      101
      5.      102
      6.      103
      7.      104
      8.      105
      9.      106
      10.      107
      11.      108
      12.      109
      13.      110
  5.   111
    1.     112
      1.      113
      2.      114
      3.      115
    2.     116
      1.      117
      2.      118
    3.     119
      1.      120
        1.       121
          1.        122
        2.       123
        3.       124
      2.      125
      3.      126
      4.      127
      5.      128
      6.      129
      7.      130
      8.      131
      9.      132
        1.       133
  6.   134
    1.     135
      1.      136
    2.     137
    3.     138
    4.     139
    5.     140
    6.     141
      1.      142
    7.     143
    8.     144
      1.      145
      2.      146
      3.      147
        1.       148
        2.       149
      4.      150
        1.       151
    9.     152
    10.     153
    11.     154
    12.     155
      1.      156
      2.      157
      3.      158
      4.      159
      5.      160
      6.      161
        1.       162
        2.       163
        3.       164
        4.       165
      7.      166
      8.      167
        1.       168
        2.       169
        3.       170
      9.      171
      10.      172
      11.      173
      12.      174
      13.      175
      14.      176
      15.      177
      16.      178
      17.      179
      18.      180
      19.      181
      20.      182
      21.      183
      22.      184
      23.      185
      24.      186
      25.      187
      26.      188
      27.      189
      28.      190
      29.      191
      30.      192
        1.       193
        2.       194
        3.       195
      31.      196
      32.      197
    13.     198
    14.     199
    15.     200
    16.     201
      1.      202
      2.      203
      3.      204
    17.     205
      1.      206
      2.      207
      3.      208
      4.      209
      5.      210
    18.     211
  7.   212
    1.     213
      1.      214
      2.      215
      3.      216
      4.      217
      5.      218
      6.      219
    2.     220
      1.      221
        1.       222
        2.       223
        3.       224
        4.       225
      2.      226
    3.     227
    4.     228
      1.      229
      2.      230
      3.      231
    5.     232
    6.     233
      1.      234
      2.      235
        1.       236
        2.       237
      3.      238
        1.       239
          1.        240
          2.        241
        2.       242
          1.        243
          2.        244
      4.      245
      5.      246
    7.     247
      1.      248
      2.      249
      3.      250
      4.      251
      5.      252
    8.     253
      1.      254
      2.      255
      3.      256
      4.      257
        1.       258
          1.        259
        2.       260
          1.        261
    9.     262
      1.      263
      2.      264
      3.      265
        1.       266
        2.       267
        3.       268
        4.       269
          1.        270
          2.        271
          3.        272
          4.        273
        5.       274
        6.       275
      4.      276
        1.       277
        2.       278
    10.     279
  8.   280
    1.     281
      1.      282
      2.      283
      3.      284
      4.      285
      5.      286
      6.      287
      7.      288
      8.      289
    2.     290
      1.      291
        1.       292
      2.      293
      3.      294
      4.      295
        1.       296
      5.      297
        1.       298
    3.     299
    4.     300
      1.      301
      2.      302
        1.       303
        2.       304
          1.        305
          2.        306
          3.        307
          4.        308
      3.      309
        1.       310
        2.       311
  9.   312
    1.     313
    2.     314
      1.      315
      2.      316
      3.      317
  10.   318
    1.     319
  11.   320
    1.     321

Extensions

Most of the GCC language extensions are available in the TI compiler when compiling in relaxed ANSI mode (--relaxed_ansi).

The extensions that the TI compiler supports are listed in Table 5-3, which is based on the list of extensions found at the GNU web site. The shaded rows describe extensions that are not supported.

Table 5-3 GCC Language Extensions

Extensions Descriptions
Statement expressions Putting statements and declarations inside expressions (useful for creating smart 'safe' macros)
Local labels Labels local to a statement expression
Labels as values Pointers to labels and computed gotos
Nested functions As in Algol and Pascal, lexical scoping of functions
Constructing calls Dispatching a call to another function
Naming types(1) Giving a name to the type of an expression
typeof operator typeof referring to the type of an expression
Generalized lvalues Using question mark (?) and comma (,) and casts in lvalues
Conditionals Omitting the middle operand of a ?: expression
Hex floats Hexadecimal floating-point constants
Complex Data types for complex numbers
Zero length Zero-length arrays
Variadic macros Macros with a variable number of arguments
Variable length Arrays whose length is computed at run time
Empty structures Structures with no members
Subscripting Any array can be subscripted, even if it is not an lvalue.
Escaped newlines Slightly looser rules for escaped newlines
Multi-line strings(1) String literals with embedded newlines
Pointer arithmetic Arithmetic on void pointers and function pointers
Initializers Non-constant initializers
Compound literals Compound literals give structures, unions, or arrays as values
Designated initializers Labeling elements of initializers
Cast to union Casting to union type from any member of the union
Case ranges 'Case 1 ... 9' and such
Mixed declarations Mixing declarations and code
Function attributes Declaring that functions have no side effects, or that they can never return
Attribute syntax Formal syntax for attributes
Function prototypes Prototype declarations and old-style definitions
C++ comments C++ comments are recognized.
Dollar signs A dollar sign is allowed in identifiers.
Character escapes The character ESC is represented as \e
Variable attributes Specifying the attributes of variables
Type attributes Specifying the attributes of types
Alignment Inquiring about the alignment of a type or variable
Inline Defining inline functions (as fast as macros)
Assembly labels Specifying the assembler name to use for a C symbol
Extended asm Assembler instructions with C operands
Constraints Constraints for asm operands
Wrapper headers Wrapper header files can include another version of the header file using #include_next
Alternate keywords Header files can use __const__, __asm__, etc
Explicit reg vars Defining variables residing in specified registers
Incomplete enum types Define an enum tag without specifying its possible values
Function names Printable strings which are the name of the current function
Return address Getting the return or frame address of a function (limited support)
Other built-ins Other built-in functions (see Section 5.17.5)
Vector extensions Using vector instructions through built-in functions
Target built-ins Built-in functions specific to particular targets
Pragmas Pragmas accepted by GCC
Unnamed fields Unnamed struct/union fields within structs/unions
Thread-local Per-thread variables
Binary constants Binary constants using the '0b' prefix.
Feature defined for GCC 3.0; definition and examples at http://gcc.gnu.org/onlinedocs/gcc-4.7.2/gcc/C-Extensions.html#C-Extensions