ZHCSSN6A August 2023 – October 2023 TPS25983
PRODUCTION DATA
Applications having two energy sources such as PCIe cards, tablets, and portable battery powered equipment require preference of one source to another. For example, mains power (wall-adapter) has the priority over the internal battery back-up power. These applications demand for switchover from mains power to backup power only when main input voltage falls below a user-defined threshold. The TPS25983 devices provide a simple design for priority power multiplexing needs.
Figure 9-17 shows a typical priority power multiplexing implementation using TPS25983 devices. When the primary (priority) power source (IN1) is present and above the undervoltage (UVLO) threshold, the primary path device path powers the OUT bus irrespective of which auxiliary supply voltage condition. The device in auxiliary path is held in off condition by forcing the OVLO pin to high using the EN/UVLO signal of the primary path device. Once the primary supply voltage falls below the user-defined undervoltage threshold (UVLO), the primary path device is turned off. At the same the auxiliary, the auxiliary path device turns on and starts delivering power to the load. In this configuration, supply overvoltage protection is not available on both channels.
The PG pins of the devices can be used as a digital indication to identify which of the two supplies is active and delivering power to the load.
A key consideration in power MUXing applications is the minimum voltage the output bus droops to during the switchover from one supply to another. This in turn depends on multiple factors including the output load current (ILOAD), output bus hold-up capacitance (COUT) and switchover time (tSW).
While switching from primary supply (VIN1) to auxiliary supply (VIN2) or vice versa, the minimum bus voltage can be calculated using Equation 30. Here, the maximum switchover time (tSW) is the time taken by the device to turn on and start delivering power to the load, which is equal to the device turn on time (tON), which includes the turn on delay (tD,ON) and rise time (tR) determined by the dVdt capacitor (CdVdt) and bus voltage.
Figure 9-18 and Figure 9-19 illustrate the power MUXing behavior.