ZHCSSN6A August 2023 – October 2023 TPS25983
PRODUCTION DATA
The TPS25983 implements Undervoltage Protection on IN to turn off the output in case the applied voltage becomes too low for the downstream load or the device to operate correctly. The Undervoltage Protection has a default internal threshold of VUVP. If needed, setting a user defined Undervoltage Protection threshold higher than VUVP using the UVLO comparator on the EN/UVLO pin is also possible. Figure 8-1 and Equation 1 show how a resistor divider from supply to GND can be used to set the UVLO set point for a given voltage supply level.
The resistors must be sized large enough to minimize the constant leakage from supply to ground through the resistor divider network. At the same time, keep the current through the resistor network sufficiently larger (20x) than the leakage current on the EN/UVLO pin to minimize the error in the resistor divider ratio.