ZHCU763 March 2021
The reference design SSR topology uses the high impedance voltage translator connected between the digital isolator and the SSR MOSFET gate. Figure 2-7 illustrates the high-impedance voltage translator consists of a PNP transistor (QP) and an NPN transistor (QN).
Figure 2-7 High Impedance Voltage
Translator for Driving Multiple SSR With Single Isolating ElementThe NPN and the PNP transistor circuit forms the voltage translator circuit, translating the 5 V at the digital isolator output to a higher voltage for the MOSFET gate drive. It is also required that the off-state leakage of the PNP transistor has to be very low so that the resulting voltage drop across the resistor between the gate and source of the SSR MOSFET, is sufficiently less than the worst-case gate threshold voltage of MOSFETs.