ZHCU602 December 2018
With a song playing, provide a swipe anywhere on the wheel in a clockwise direction to select the next song. Swipe in a counter-clockwise to select the previous song. Experiment with the starting position. You should see this function works independent of where you start the gesture.
NOTE
The wheel resolution is 100 points. The swipe gesture requires that your finger move a minimum distance of 10 points.
It is also possible to select the next or previous songs with a tap gesture on the regions shown in Figure 12.