ZHCU602 December 2018
A double-tap gesture is defined as a momentary finger touch followed by a release, then a second touch and release. Figure 8 shows that the double-tap gesture is essentially a tap followed by a delay that defines a window when the second touch can occur. The software parameters are TouchSampleCount_Min, TouchSampleCount_Max and DoubleTapDelayCount_Max.
NOTE
A sensor that supports double-tap also supports tap by default. The reader must be aware that if a tap and not a double-tap is detected, the tap gesture is not reported until after the double-tap delay period expires. This can create a slight delay in tap response, but when properly tuned, the delay has a minimal impact on user interaction.
Figure 8. Double Tap Gesture Detection