SWRU641 March 2026
The RF path of the two WM devices on the CC2662R-Q1 by default use the Inverted F antenna printed on the PCB. The SMA connector near the PCB antenna of each WM can be used instead, which is useful for tests using an external antenna or for RF-conducted measurements.
For WM#1 capacitor C43 must be desoldered from it's original horizontal position and resoldered vertically (in the C39 position) to connect to the pad routed to the SMA J4. WM1 Conducted Setup shows the location of the caps and SMA connector J4.
Figure 3-1 WM1 Conducted SetupFor WM#2 capacitor C83 must be desoldered from it's original horizontal position and resoldered vertically (in the C79 position) to connect to the pad routed to the SMA J11. WM2 Conducted Setup shows the location of the caps and SMA connector J11.
Figure 3-2 WM2 Conducted Setup