SWRU570B May 2021 – December 2021 WL1801 , WL1801MOD , WL1805MOD , WL1807MOD , WL1831 , WL1831MOD , WL1835MOD , WL1837MOD
The WiLink™ Wireless Tools package contains several tools for both Bluetooth and WLAN evaluation using PC environment. The package contains the following tools.
| Technology | Tool Name | Utility | |
|---|---|---|---|
| WLAN | WLAN Real-Time Tuning Tool (RTTT) | RF system debug and calibration software tool | |
| WLAN gLogger | Records messages from the WiLink WLAN firmware. More details can be found at WiLink™ WLAN gLogger Tool | ||
| Bluetooth/Bluetooth low energy | HCITester Tool | enables HCI testing capabilities for TI Bluetooth devices | |
| BTSout | Sends the BTS to the device on a specified port and baud rate | ||
| BTSTransform | Converts the BTS format to Hex command strings | ||
| ScriptPad | Allows the text file to be saved in BTS format in the HCI tester | ||
| Bluetooth Logger | Traces log messages generated by the Bluetooth host controller and monitors protocol transactions. More details on the usage of the tool is provided at Bluetooth® Logger and Link Quality Monitor (LQM) Tools | ||
| Link Quality Monitor (LQM) | Monitors system behavior using the received signal strength indication (RSSI), link throughput, and adaptive frequency hopping (AFH) map table of all active Bluetooth and Bluetooth low-energy links in run time | ||
TI Wireless Tools Package Getting Started Guide provides the details of installation, functionality and operation of each of the tools contained in the Wireless Tools package.