SWRU509 February   2017 CC3200

 

  1.   SimpleLinkrep%#8482; Wi-Fi® SensorTag
    1.     Trademarks
    2. 1 Introduction
      1. 1.1 CC3200 SensorTag
      2. 1.2 Key Features
      3. 1.3 What is Included
      4. 1.4 FCC/IC Regulatory Compliance
        1. 1.4.1 FCC
          1. 1.4.1.1 Class B Operation
          2. 1.4.1.2 RF Exposure Information (SAR)
        2. 1.4.2 IC
          1. 1.4.2.1 RF Exposure Information (SAR)
        3. 1.4.3 EU
          1. 1.4.3.1 RF Exposure Information (SAR)
    3. 2 Hardware Description
      1. 2.1 Block Diagram
      2. 2.2 Hardware Features
      3. 2.3 RF Function and Frequency Range
      4. 2.4 Sensors and Peripherals
        1. 2.4.1 Reed Relay
        2. 2.4.2 Digital Microphone
        3. 2.4.3 Buzzer
        4. 2.4.4 Gyroscope, Accelerometer, and Compass
        5. 2.4.5 Infrared Thermopile Sensor
        6. 2.4.6 Pressure Sensor
        7. 2.4.7 Humidity Sensor
        8. 2.4.8 Light Sensor
    4. 3 Operation Description
      1. 3.1 Downloading the SensorTag App
      2. 3.2 Setting Up the SensorTag as an Access Point
        1. 3.2.1 First-Time Configuration Only
      3. 3.3 Connecting the SensorTag to Your Local Wi-Fi Network
      4. 3.4 Switching Between Modes
      5. 3.5 Troubleshooting
      6. 3.6 Replacing the Batteries
    5. 4 Design Files
      1. 4.1 Hardware
    6. 5 PCB Revision
    7. 6 References
  2.   Revision History

First-Time Configuration Only

On your mobile phone, go to the Settings menu and connect to the SensorTag-xx access point (see Figure 3). The -xx value is the two last digits of the SensorTag MAC address; this value is used to uniquely identify your SensorTag.

Connecting the phone to the access point may take up to 30 seconds the first time it connects.

NOTE

Only one device can be connected to the Wi-Fi SensorTag when it is configured as an access point. On some phone models, the 4G connection and 5-GHz Wi-Fi must be disabled to detect the SensorTag as access point.

swru503_example_of_sensortag_access.gifFigure 3. Example of SensorTag Access Point

To launch the SensorTag app, you may have to pull down the menu in the SensorTag device list to refresh the device list. The app detects the new Wi-Fi SensorTag. If the SensorTag is programmed with firmware version 0.98, the app will prompt you to upgrade the SensorTag to the latest version (see Figure 4). Follow the steps to upgrade the SensorTag.

If an upgrade has already taken place and a newer firmware version becomes available, users must first revert back to the factory default (firmware version 0.98). This can be done in one of 2 ways:

  • In the mobile application, select Firmware Upgrade → Factory Default.
  • or

  • Depress the two SensorTag hardware buttons simultaneity for a few seconds until the beep sound is activated.

swru509_wifi_ota_upgrade.gifFigure 4. Wi-Fi® OTA Upgrade

From the firmware upgrade screen, go back to the SensorTag device list screen (see Figure 5 and Figure 6).

  • For IOS® devices, go into Settings and manually reconnect to the SensorTag-xx access point.
  • For Android devices, the phone will keep the connection to the SensorTag access point. On the Android device, select Configure new Wi-Fi SensorTag, and follow the on-screen instructions to configure the Wi-Fi settings.
swru509_configuring_new_device_01.gifFigure 5. Available Device
swru509_configuring_new_device_02.gifFigure 6. New Device Found