SWRU497B August   2019  – December 2021 CC2564C

 

  1.   Trademarks
  2. 1Introduction
  3. 2Features
    1. 2.1 Classic Bluetooth Profiles Available
    2. 2.2 Bluetooth Low Energy Profiles Available
    3. 2.3 MFi Support
  4. 3Requirements
  5. 4Sample Application Overview
  6. 5Hardware Setup
    1. 5.1 Setting Up the Hardware
  7. 6Software Setup
    1. 6.1 Downloading and Installing
    2. 6.2 Building and Flashing the Bluetooth Code (MSP-EXP432P401R)
  8. 7Sample Applications
    1. 7.1 Classic Bluetooth Sample Applications
    2. 7.2 Classic Bluetooth + Bluetooth Low Energy Sample Applications
    3. 7.3 Bluetooth Low Energy Sample Applications
  9. 8Revision History

Setting Up the Hardware

To set up the hardware, do as follows:

  1. Fit the CC256XCQFN-EM on the EM BoosterPack Adapter (BOOST-CCEMADAPTER).
  2. Stack the BOOST-CCEMADAPTER onto the MSP432 LaunchPad (MSP-EXP432P401R).
    Note: The boards must be set to their default settings.

    For more information on the jumper positions and default settings for the BOOST-CCEMADAPTER, see the CC256XCQFNEM Quick Start Guide and the Dual-Mode Bluetooth CC2564C QFN EM User's Guide. For jumper positions and configurations for the MSP-EXP432P401R development kit, see the MSP432 LaunchPad Development Kit User's Guide.

    Ensure that the connectors of the LaunchPad and the BOOST-CCEMADAPTER are aligned.

  3. To use the CC3200AUDBOOST device for audio and voice applications (optional), do as follows:
    • Ensure that the directions of the PCM signals are properly set on the CC256XCQFN-EM to evaluate audio and voice sample applications. The directions of the PCM signals can be configured so that the PCM port on the CC2564C device is either PCM master or PCM slave, depending on the sample application. See Table 5-1 to ensure that the R18, R19, and R11 on the CC256XCQFN-EM are properly configured for complete evaluation of the audio and voice sample applications.
      Table 5-1 CC256XCQFN-EM PCM Direction for Audio and Voice Sample Applications
      Demo Name CC256XCQFN-EM
      PCM Role
      R18(1) R19(1) R11(1)
      A3DP Demo_SNK Master (Default) DNI 10K Ω 0 Ω or DNI
      A3DP Demo_SRC,
      HFP Demo_AG,
      HFP Demo_HF,
      and HSP Demo
      Master DNI 10K Ω DNI
      DNI indicates Do not install.

      Figure 5-1 shows the position of the R18, R19, and R11 resistors on the CC256XCQFN-EM board.

      GUID-7BCCFA39-03AD-4C29-8A5F-A85332ED85AF-low.gif Figure 5-1 CC256XCQFN-EM PCM Role Selection for Audio and Voice Sample Applications

      For more details regarding the PCM role selection on the CC256XCQFN-EM board, refer to CC256xCQFN-EM User's Guide and Dual-Mode Bluetooth® CC2564CQFN-EM Evaluation Board.

    • Connect the CC3200AUDBOOST audio codec board to the BOOST-CCEMADAPTER and the MSP-EXP432P401R, as shown in Figure 5-2.
    Note:

    Because the BOOST-CCEMADAPTER and CC3200AUDBOOST BoosterPack pinouts conflict with each other, the CC3200AUDBOOST cannot be stacked on the MSP432 LaunchPad while the BOOST-CCEMADAPTER is being used. Minor prototyping and jumper wire connections are required to connect the CC3200AUDBOOST with the BOOST-CCEMADAPTER and the MSP-EXP432P401R.

GUID-B4DF3CC6-36D6-4C60-A802-26C26BBC250F-low.gif GUID-D8020154-E189-4A6E-9524-CDA9D7E170BE-low.png Figure 5-2 CC3200AUDBOOST Connection With BOOST-CCEMADAPTER and MSP-EXP432P401R
Table 5-2 CC3200AUDBOOST Ports or Audio Sample Applications
Sample Applications CC3200AUDBOOST Port
A3DP Demo_SRC LINE_IN (J3)
A3DP Demo_SNK LINE_OUT (J4)
HFP Demo_AG Mic (U6)
LINE_OUT (J4)
HFP Demo_HF Mic (U6)
LINE_OUT (J4)
HSP Demo Mic (U6)
LINE_OUT (J4)
Note: For the default settings for the CC3200AUDBOOST device, see the CC3200 SimpleLink™ Wi-Fi® and IoT Solution, a Single Chip Wireless MCU - Audio BoosterPack user's guide. Ensure the reliability of the connections that are shown in Figure 5-2.

For more details regarding the PCM role selection on the CC256XCQFN-EM board, see the CC256xCQFN-EM User's Guide and Dual-Mode Bluetooth® CC2564CQFN-EM Evaluation Board.