SWRA657 June   2020 CC3100 , CC3200

 

  1.   SimpleLink Wi-Fi CC3100, CC3200 Serial Flash
    1.     Trademarks
    2. 1  Introduction
    3. 2  How File System Content Gets to the Serial Flash
    4. 3  File System Guidelines
    5. 4  User File Mathematics
    6. 5  System and Configuration Files
      1. 5.1 Description
      2. 5.2 Memory Consumption
        1. 5.2.1 CC3200 Use Case
        2. 5.2.2 Host Driver Mapping
        3. 5.2.3 Minimum Flash Size
    7. 6  Implementing File System Features From Host Processor
      1. 6.1 Overview
      2. 6.2 File Listing
        1. 6.2.1 Requirements
        2. 6.2.2 Procedure
      3. 6.3 Free/Occupied Space
        1. 6.3.1 Requirements
        2. 6.3.2 Procedure
      4. 6.4 File Appending
        1. 6.4.1 Requirements
        2. 6.4.2 Procedure
    8. 7  Factors to Consider in Designing With Serial Flash
      1. 7.1 Serial Flash Vendor and Part Number Selection
      2. 7.2 Supported Flash Types
      3. 7.3 Frequent Write Operations
        1. 7.3.1 Serial Flash Access by the Wi-Fi System"
        2. 7.3.2 Seral Flash Access by the WiFi System
          1. 7.3.2.1 System Files
          2. 7.3.2.2 User Files
      4. 7.4 Sudden Power Off (power removal during a write/erase phase)
        1. 7.4.1 Battery Powered Systems
        2. 7.4.2 Line Powered Systems
    9. 8  Design Recommendations for Ensuring the Integrity of the Power Supply to the Serial Flash
      1. 8.1 Overview
      2. 8.2 Key Points
      3. 8.3 Brown-Out Mitigation Techniques for New Self-Hosted CC3200 Designs
    10. 9  Recommended Best Practices
    11. 10 Implications of Data Integrity Compromise to CC3100/CC3200
      1. 10.1 Recovery
    12. 11 References

Procedure

The procedure for listing the files and their respective allocated space is as follows:

  1. Keep the following information for every user file created:
    1. Filename
    2. Calculate file size according to Section 4.
  2. Loop over all user files and print:
    1. Filename
    2. Calculated size
  3. Loop over all system/configuration files, invoke fsGetInfo() API and conclude:
    1. If return value is SL_FS_ERR_FILE_NOT_EXISTS, file does not exist and thus should not be printed. Else, the file exists and should be printed along with the allocated size
    2. If return value is SL_FS_ERR_TOKEN_IS_NOT_VALID, it means the file is secured but exists. This return value applies to the following three files:
      1. /tmp/fcon.frm
      2. /sys/pref.net
      3. /sys/smartconfigkeys.cfg

In this case, the file exists and should be printed along with the allocated size.

Figure 2 illustrates the procedure.

swra657-file-listing-flow.gifFigure 2. File Listing Flow