SWPA230A May 2017 – June 2018 CC3120 , CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
Programming the patches to the SRAM is applied in chunks. The chunk size is 4096 bytes but the maximal size that can be programmed is 4080 bytes. Thus, the buffer is programmed in actual chunks of 4080 bytes. The procedure for programming the SRAM follows:
Figure 9 shows the SRAM programming procedure in a zoomed-out pane. As observed, the procedure is divided into three separate programming instances.
Figure 9. Raw Storage Write to SRAM (Zoomed Out) Figure 10 shows the SRAM programming procedure in a zoomed-in pane to the second chunk. As observed, the chunk is 4080 bytes in offset 4080.
Figure 10. Raw Storage Write to SRAM (Zoomed In)