SWPA230A May 2017 – June 2018 CC3120 , CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
Programming the patches to the SFLASH is applied in chunks. The chunk size is 4096 bytes but the maximal size that can be programmed is 4080 bytes. Thus, the buffer is programmed in actual chunks of 4080 bytes. The procedure for programming the SFLASH follows:
Figure 13 shows the SFLASH programming procedure in a zoomed-out pane. As observed, the procedure is divided into three separate programming instances.
Figure 13. Raw Storage Write to SFLASH (Zoomed Out) Figure 14 shows the SFLASH programming procedure in a zoomed-in pane to the first chunk. As observed, the chunk is 4080 bytes in offset (33 × 4096 + 8 = 135176 bytes).
Figure 14. Raw Storage Write to SFLASH (Zoomed In)