SPRZ457J January 2021 – October 2025 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
Boot: UART Backup Boot Authentication Failure w/ xSPI Primary Boot Mode
On HS-SE device type using a flash based primary boot mode which support redundant boot address like OSPI boot mode and a secondary boot mode like UART. Under the following condition:
Boot a valid image from backup boot media (UART) with below configuration:
ROM is not able to boot the Valid image from the secondary boot mode, like UART boot media.
Under normal circumstance, after each time an image failed to boot, Secure ROM has to reset all the internal state machine for the next Retry operation.
When trying operate on the TIFS certificate, Secure ROM doesn’t reset all the necessary variables after the Image failed at Redundant offset.
Hence, during Backup boot flow Secure ROM was not able to authenticate the Certificate/Image binary.
Due to this, Boot fails at UART backup boot for a Valid Image binary as well.
None, other than making sure the image located at the redundant offset is a complete boot certificate and not just a TIFS/SYSFW certificate.