SPRZ452I july   2018  – may 2023 AM6526 , AM6528 , AM6546 , AM6548

 

  1. 1Usage Notes and Advisories Matrices
  2. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development-Support Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  3. 3Silicon Revision 2.1, 2.0, 1.0 Usage Notes and Advisories
    1. 3.1 Silicon Revision 2.1, 2.0, 1.0 Usage Notes
      1. 3.1.1 Fail-Safe IO's: Latch-up Risk on Fail-Safe IOs
      2. 3.1.2 ADC: High Input Leakage Current May Impact ADC Accuracy
      3. 3.1.3 INTRTR: Spurious Interrupts Generated when Programming Certain Interrupt Routers
      4.      i2351
    2. 3.2 Silicon Revision 2.1, 2.0, 1.0 Advisories
      1. 3.2.1 Silicon Revision 2.1, 2.0, 1.0 Advisory List
      2.      i939
      3.      i2000
      4.      i2004
      5.      i2006
      6.      i2009
      7.      i2013
      8.      i2015
      9.      i2018
      10.      i2019
      11.      i2020
      12.      i2021
      13.      i2022
      14.      i2023
      15.      i2024
      16.      i2025
      17.      i2026
      18.      i2027
      19.      i2028
      20.      i2030
      21.      i2032
      22.      i2037
      23.      i2038
      24.      i2039
      25.      i2046
      26.      i2053
      27.      i2054
      28.      i2055
      29.      i2068
      30.      i2069
      31.      i2073
      32.      i2075
      33.      i2076
      34.      i2083
      35.      i2084
      36.      i2095
      37.      i2096
      38.      i2097
      39.      i2098
      40.      i2099
      41.      i2101
      42.      i2103
      43.      i2104
      44.      i2106
      45.      i2115
      46.      i2116
      47.      i2118
      48.      i2119
      49.      i2129
      50.      i2132
      51.      i2137
      52.      i2138
      53.      i2139
      54.      i2141
      55.      i2143
      56.      i2146
      57.      i2148
      58.      i2149
      59.      i2161
      60.      i2162
      61.      i2164
      62.      i2165
      63.      i2177
      64.      i2184
      65.      i2185
      66.      i2187
      67.      i2189
      68.      i2193
      69.      i2196
      70.      i2198
      71.      i2204
      72.      i2207
      73.      i2231
      74.      i2234
      75.      i2245
      76.      i2307
      77.      i2014
      78.      i2145
      79.      i2163
      80.      i2173
      81.      i2249
      82.      i2278
      83.      i2279
      84.      i2307
      85.      i2310
      86.      i2311
      87.      i2320
      88.      i2328
      89.      i2329
      90.      i2040
      91.      i2041
      92.      i2043
      93. 3.2.2 i2151
      94.      i2262
      95.      i2264
      96.      i2265
      97.      i2266
      98.      i2268
      99.      i2312
      100.      i2371
        1.       Trademarks
          1.        Revision History

i2041

PCIe: Calculated Negative Round-trip Time Causes Wrong PTM Requester Local time

Details:

PTM Master Time is calculated by the Requester using the round trip time for PTM request and response (Requester to Responder and back). If the calculated round trip time is negative, it causes the Requester local clock to have a huge offset of 2^63 nanoseconds.

The following is the equation used to calculate PTM Master Time (same as PTM Requester local clock):

PTM Master Time at t1’ = t2’ – round_trip/2

Where round_trip = ((t4-t1) – (t3-t2))

Please note that t1 is the estimated time for PTM Request at the Requester’s upstream port. This includes the local time added with the programmed MAC and PHY latencies for transmit. Similarly t4 is the estimated time for PTM Response and the Requester’s upstream port. This includes local time subtracted by the programmed MAC and PHY latencies for receive.

PTM Master Time calculated after receiving ResponseD message is then used to update the Requester’s local clock.

Round trip time can become negative if (t3-t2) is greater than (t4-t1). This can happen if either or both of below scenarios happen:

1. PTM Requester’s transmit and receive latency registers are programmed with values that are close to or greater than actual PHY and MAC latency.

2. The clock frequencies between Requester’s Upstream port and Responder’s Downstream port have significant difference and the actual wire delays between these two ports are short (few nanoseconds).

The issue arises because the round trip time is stored as an unsigned number and is right shifted to create the divide by two value. As a result, round_trip/2 component in the PTM Master Time equation becomes a very large positive number. This leads to the following issues:

1. 2^63 nanoseconds offset in the adjusted Requester’s local clock going to CPTS for hardware push.

2. The VSEC PTM registers have this offset as well. The affected PTM registers are PCIE_EP_PTM_REQ_LOCAL_LSB_OFF, PCIE_EP_PTM_REQ_LOCAL_MSB_OFF, PCIE_EP_PTM_REQ_T1_LSB_OFF, PCIE_EP_PTM_REQ_T1_MSB_OFF, PCIE_EP_PTM_REQ_T1P_LSB_OFF, PCIE_EP_PTM_REQ_T1P_MSB_OFF, PCIE_EP_PTM_REQ_T4_LSB_OFF, PCIE_EP_PTM_REQ_T4_MSB_OFF, PCIE_EP_PTM_REQ_T4P_LSB_OFF, PCIE_EP_PTM_REQ_T4P_MSB_OFF.

Workaround(s):

One of the following workarounds have to be implemented:

1. Program the transmit latency (PCIE_EP_PTM_REQ_TX_LATENCY_OFF register) and receive latency (PCIE_EP_PTM_REQ_RX_LATENCY_OFF) to zero. This will eliminate the issue as long as clock drift between Requester/EP and Responder/RC is less than 4100pm. However, this workaround will increase the deviation for Requester clock with respect to Responder’s PTM Master Time.

2. Detect and correct for this 2^63 nanoseconds offset: -

  • Ignore bits 63 and 62 of the local clock and timestamps in VSEC PTM register space.
  • Do not set PTM_CLK_SEL field in PTMCFG register to values of 62 or 63. This will prevent the CPTS hardware push logic from using the two most significant bits of the PTM local clock. This limits maximum PTM time to less than 136 years.