SPRZ171T December 2004 – September 2020 SM320F2801-EP , SM320F2808-EP , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F2806 , TMS320F2806-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2809-Q1
Figure 3-1 provides an example of the TMS320F280x device markings and defines each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 3-1. Some prototype devices may have markings different from those illustrated. Figure 3-2 shows an example of device nomenclature.
Figure 3-1 Example of Device Markings
Figure 3-2 Example of Device Nomenclature| SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | F2809 COMMENTS |
|---|---|---|---|
| Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMS. |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
| SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | C2801, C2802 COMMENTS |
|---|---|---|---|
| Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX only. |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMS. |
| SILICON REVISION CODE | SILICON REVISION | REVISION ID Address: 0x0883 | F2801, F2802, F2806, and F2808 COMMENTS | F28015 and F28016 COMMENTS |
|---|---|---|---|---|
| Blank (no second letter in prefix) | Indicates Revision 0 | 0x0000 | This silicon revision is available as TMX only. | TI internal only |
| A | Indicates Revision A | 0x0001 | This silicon revision is available as TMX only. | TI internal only |
| B | Indicates Revision B | 0x0002 | This silicon revision is available as TMS. | TI internal only |
| C | Indicates Revision C | 0x0003 | This silicon revision is available as TMS. | This silicon revision is available as TMS. |