SPRZ171T December   2004  – September 2020 SM320F2801-EP , SM320F2808-EP , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F2806 , TMS320F2806-Q1 , TMS320F2808 , TMS320F2808-Q1 , TMS320F2809 , TMS320F2809-Q1

 

  1. 1Introduction
  2. 2Device and Development Tool Support Nomenclature
  3. 3Device Markings
  4. 4Silicon Change Overview
  5. 5Usage Notes and Known Design Exceptions to Functional Specifications
    1. 5.1 Usage Notes
      1. 5.1.1 PIE: Spurious Nested Interrupt After Back-to-Back PIEACK Write and Manual CPU Interrupt Mask Clear Usage Note
    2. 5.2 Known Design Exceptions to Functional Specifications
      1.      Advisory
      2.      Advisory
      3.      Advisory
      4.      Advisory
      5.      Advisory
      6.      Advisory
      7.      Advisory
      8.      Advisory
      9.      Advisory
      10.      Advisory
      11.      Advisory
      12.      Advisory
      13.      Advisory
      14.      Advisory
      15.      Advisory
      16.      Advisory
      17.      Advisory
      18.      Advisory
      19.      Advisory
      20.      Advisory
      21.      Advisory
      22.      Advisory
  6. 6Documentation Support
  7. 7Trademarks
  8. 8Revision History

PIE: Spurious Nested Interrupt After Back-to-Back PIEACK Write and Manual CPU Interrupt Mask Clear Usage Note

Revision(s) Affected:0, A on F2809 silicon
0, A on C280x silicon
0, A, B, C on F2801, F2802, F2806, F2808, and F2801x silicon

Certain code sequences used for nested interrupts allow the CPU and PIE to enter an inconsistent state that can trigger an unwanted interrupt. The conditions required to enter this state are:

  1. A PIEACK clear is followed immediately by a global interrupt enable (EINT or asm(" CLRC INTM")).
  2. A nested interrupt clears one or more PIEIER bits for its group.

Whether the unwanted interrupt is triggered depends on the configuration and timing of the other interrupts in the system. This is expected to be a rare or nonexistent event in most applications. If it happens, the unwanted interrupt will be the first one in the nested interrupt's PIE group, and will be triggered after the nested interrupt re-enables CPU interrupts (EINT or asm(" CLRC INTM")).

Workaround: Add a NOP between the PIEACK write and the CPU interrupt enable. Example code is shown below.


     //Bad interrupt nesting code
     PieCtrlRegs.PIEACK.all = 0xFFFF;      //Enable nesting in the PIE
     EINT;                                 //Enable nesting in the CPU
  
     //Good interrupt nesting code
     PieCtrlRegs.PIEACK.all = 0xFFFF;      //Enable nesting in the PIE
     asm(" NOP");                          //Wait for PIEACK to exit the pipeline
     EINT;                                 //Enable nesting in the CPU