SPRUI78D March 2019 – January 2022 F28377D-SEP , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
The CLA co-processor has built in mechanisms to detect execution of an illegal instruction (illegal opcode), floating point underflow or overflow conditions. CLA will interrupt CPU under such conditions. Any access to an invalid memory range will return 0x00000000 data. Access to an erased flash (default state for a new device) will return 0xFFFFFFFF. Both 0x00000000 and 0xFFFFFFFF are decoded as invalid instructions so that an erased flash, cleared memory, or an invalid address will generate an interrupt to CPU. CPU can decode the interrupt cause by checking the required CLA flags. Error response, diagnostic testability, and any necessary software requirements are defined by the software implemented by the system integrator.