SPRUI78D March 2019 – January 2022 F28377D-SEP , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S
The power-on reset (PORn) generates an internal warm reset signal to reset the majority of digital logic as part of the boot process. The warm reset can also be provided at device level as an I/O pin (XRSn) with open drain implementation. Diagnostic capabilities like NMI watchdog and Watchdog are capable of issuing a warm reset. For more information on the reset functionality, see the device-specific data sheet.
The following tests can be applied as diagnostics for this module to provide diagnostic coverage on a specific function.
The following tests can be applied as test-for-diagnostics on this module to meet Latent Fault Metric Requirements: