SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
Figure 20-17 Conceptual Block Diagram of the Sample Rate GeneratorThe source clock for the sample rate generator (labeled CLKSRG in the diagram) can be supplied by the LSPCLK, or by an external pin (MCLKX or MCLKR ). The source is selected with the SCLKME bit of PCR and the CLKSM bit of SRGR2. If a pin is used, the polarity of the incoming signal can be inverted with the appropriate polarity bit (CLKXP of PCR or CLKRP of PCR).
The sample rate generator has a three-stage clock divider that gives CLKG and FSG programmability. The three stages provide:
The McBSP cannot operate at a frequency faster than ½ the source clock frequency. You must choose an input clock frequency and a CLKGDV value such that CLKG is less than or equal to ½ the source clock frequency.
In addition to the three-stage clock divider, the sample rate generator has a frame-synchronization pulse detection and clock synchronization module that allows synchronization of the clock divide down with an incoming frame-synchronization pulse on the FSR pin. This feature is enabled or disabled with the GSYNC bit of SRGR2.
For details on getting the sample rate generator ready for operation, see Section 20.4.4.