SPRUHX5I August 2014 – May 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
Table 3-341 lists the memory-mapped registers for the DCSM_Z2_OTP registers. All register offset addresses not listed in Table 3-341 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | Z2OTP_LINKPOINTER1 | Zone 2 Link Pointer1 in Z2 OTP | Go | |
| 4h | Z2OTP_LINKPOINTER2 | Zone 2 Link Pointer2 in Z2 OTP | Go | |
| 8h | Z2OTP_LINKPOINTER3 | Zone 2 Link Pointer3 in Z2 OTP | Go | |
| 10h | Z2OTP_PSWDLOCK | Secure Password Lock in Z2 OTP | Go | |
| 14h | Z2OTP_CRCLOCK | Secure CRC Lock in Z2 OTP | Go | |
| 1Eh | Z2OTP_BOOTCTRL | Boot Mode in Z2 OTP | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-342 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
Z2OTP_LINKPOINTER1 is shown in Figure 3-299 and described in Table 3-343.
Return to the Summary Table.
Zone 2 Link Pointer1 in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_LINKPOINTER1 | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_LINKPOINTER1 | R | FFFFFFFFh | Zone2 Link Pointer 1 location in USER OTP. Reset type: SYSRSn |
Z2OTP_LINKPOINTER2 is shown in Figure 3-300 and described in Table 3-344.
Return to the Summary Table.
Zone 2 Link Pointer2 in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_LINKPOINTER2 | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_LINKPOINTER2 | R | FFFFFFFFh | Zone2 Link Pointer 2 location in USER OTP. Reset type: SYSRSn |
Z2OTP_LINKPOINTER3 is shown in Figure 3-301 and described in Table 3-345.
Return to the Summary Table.
Zone 2 Link Pointer3 in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_LINKPOINTER3 | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_LINKPOINTER3 | R | FFFFFFFFh | Zone2 Link Pointer 3 location in USER OTP. Reset type: SYSRSn |
Z2OTP_PSWDLOCK is shown in Figure 3-302 and described in Table 3-346.
Return to the Summary Table.
Secure Password Lock in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_PSWDLOCK | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_PSWDLOCK | R | FFFFFFFFh | Zone2 password lock location in USER OTP. Reset type: SYSRSn |
Z2OTP_CRCLOCK is shown in Figure 3-303 and described in Table 3-347.
Return to the Summary Table.
Secure CRC Lock in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_CRCLOCK | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_CRCLOCK | R | FFFFFFFFh | Zone2 CRC lock location in USER OTP. Reset type: SYSRSn |
Z2OTP_BOOTCTRL is shown in Figure 3-304 and described in Table 3-348.
Return to the Summary Table.
Boot Mode in Z2 OTP
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| Z2OTP_BOOTCTRL | |||||||||||||||||||||||||||||||
| R-FFFFFFFFh | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | Z2OTP_BOOTCTRL | R | FFFFFFFFh | Zone2 Boot control location in USER OTP. Reset type: SYSRSn |