SPRACP6 December 2019 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
On every reset, the device executes a boot sequence in ROM depending on the boot mode configuration. By default, the boot ROM uses two boot control GPIO pins to determine the boot mode configuration. Table 1 shows the default boot mode options of the F28004x device.
| Boot Mode | GPIO24 (default boot mode select pin 1) | GPIO32 (default boot mode select pin 0) |
|---|---|---|
| Parallel IO | 0 | 0 |
| SCI/Wait boot | 0 | 1 |
| CAN | 1 | 0 |
| Flash | 1 | 1 |
There are two ways the boot control GPIO pins can be re-purposed for use in an application: