SNLA267A March   2019  – June 2019 DS90UB953-Q1 , DS90UB954-Q1 , DS90UB960-Q1

 

  1.   How to Design a FPD-Link III System Using DS90UB953-Q1 and DS90UB954-Q1
    1.     Trademarks
    2. 1 Overview
      1. 1.1 System Level Functionality
    3. 2 Basic Design Rules
      1. 2.1 IDX and MODE Pin Verification
        1. 2.1.1 REF Clock, CLK IN, AON and Frequency Selection
          1. 2.1.1.1 Synchronous Mode
          2. 2.1.1.2 Non-Synchronous CLK_IN Mode
          3. 2.1.1.3 Non-Synchronous AON Mode
          4. 2.1.1.4 CSI Throughput
          5. 2.1.1.5 Clocking and Frequency Selection Example
      2. 2.2 Successful I2C Communication With 953 and 954
        1. 2.2.1 Aliasing
        2. 2.2.2 Port Selection on 954
      3. 2.3 I2C Passthrough Verification
      4. 2.4 Basic Diagnostic and Error Registers
    4. 3 Designing the Link Between SER and DES
      1. 3.1 Back Channel Configuration
      2. 3.2 BIST
        1. 3.2.1 BIST Configuration and Status
        2. 3.2.2 BIST Procedure
        3. 3.2.3 List of Registers Used in BIST Script
      3. 3.3 AEQ
      4. 3.4 CML Out
    5. 4 Designing Link Between SER and Image Sensor
      1. 4.1 Sensor Initialization Using SER GPIOs
      2. 4.2 CLKOUT
    6. 5 Designing Link Between DES and ISP
      1. 5.1 Frame Sync
        1. 5.1.1 Using SER GPIOs From the DES
        2. 5.1.2 Internal and External Frame Sync Configuration
        3. 5.1.3 Tables for Using GPIOs and Frame Sync
      2. 5.2 Port Forwarding
      3. 5.3 Pattern Generation
        1. 5.3.1 Accessing Indirect Registers
        2. 5.3.2 Pattern Generation From DES to ISP and SER to DES
    7. 6 Hardware Design
      1. 6.1 Basic I2C Connectors
        1. 6.1.1 I2C Pullups for SDA and SCL
      2. 6.2 AC Capacitor on FPD3 Link
      3. 6.3 Capacitance Used in Loop Filter
      4. 6.4 Critical Signal Routing
      5. 6.5 Time Domain Reflection
      6. 6.6 Return Loss and Insertion Loss
      7. 6.7 Power-over-Coax (PoC)
      8. 6.8 Voltage and Temperature Sensing
    8. 7 Appendix
      1. 7.1 Scripts
        1. 7.1.1  BIST Script
        2. 7.1.2  Example Sensor Initialization Script
        3. 7.1.3  CSI Enable and Port Forwarding Script
        4. 7.1.4  Enabling CMLOUT FPD3 RX Port 0 on 954
        5. 7.1.5  Remote Enabled SER GPIO Toggle Script
        6. 7.1.6  Local SER GPIO Toggle Script
        7. 7.1.7  Internal FrameSync on 953 GPIO1
        8. 7.1.8  External FrameSync on 953 GPIO0
        9. 7.1.9  SER GPIOs as Inputs and Output to DES GPIO
        10. 7.1.10 Pattern Generation on the 953 Script
        11. 7.1.11 Pattern Generation on the 954 Script
        12. 7.1.12 Monitor Errors for Predetermined Time Script
        13. 7.1.13 954 and 953 CSI Register Check Script
        14. 7.1.14 Time Till Lock Script on 953
      2. 7.2 Acknowledgments
  2.   Revision History

AC Capacitor on FPD3 Link

typical_application_ds90ub953-q1_snls547.gifFigure 20. Simplified Block Diagram of DS90UB953-Q1/DS90UB954-Q1 System

The DS90UB953-Q1 FPD-Link III architecture is a 40-bit frame, high-speed synchronous back channel when communicating with 954 and 960. However, the mode that the device is operating in can change the data rate of the serial data output signal. For synchronous mode where the reference oscillator is provided by the deserializer, the serial data rate is 4 Gbps presented as a differential CML output on the DOUTP and DOUTN pins.

As shown in Figure 20, the signals at DOUTP and DOUTN must be AC-coupled with a series capacitor before the interconnect that leads to the deserializer. This AC-coupling capacitor will have a value of 0.033 μF when the device is running in 4-Gbps mode. At lower data rates, a larger coupling cap will be required. When connecting to a coax cable, the AC-coupling cap on the dummy side of the output (DOUTN) should also have an AC-coupling capacitor. This value should be half of the AC-coupling cap going to the cable (0.015 µF), and DOUTN should have a 50-Ω load on DOUTN. This load is needed because the AC and DC loads seen by DOUTP and DOUTN should be balanced. The capacitor on DOUTN should be half the value of the capacitor on DOUTP because the signal path must be balanced for the AC-coupling cap near the serializer and deserializer ends of the cable.

As mentioned previously, the AC capacitors will change if either the 953 or 954 are interfaced with lower data-rate parts such as 913A, 914A, 933, and 934. With a lower data-rate, the frequency band of interest is now lower in frequency and requires a larger capacitor.