SLVUD80 September 2025
The EVM contains one row of ten 2-pin jumpers (J2), which are removable to isolate the microcontroller resource as a controlling source to the power stage. If a particular signal is interfaced externally, attach the controlling signal to either the test stakes or the driver side of J2.
Figure 3-6 DRV8844A Jumpers