SLVUD80 September 2025
This EVM offers access to the Motor Voltage (VM) power rail via a terminal block (J4). A set of test clips in parallel with the terminal block allows monitoring of the input power rail.
Since the DRV8844A can be utilized with either split power supplies (+VM/VNEG) or with a single power supply (+VM), jumpers on J5 allow the LGND and VNEG nodes to be connected together when using the single power-supply implementation.
The VM must be applied according to the parameters recommended in the DRV8844A data sheet.
NOTE: Due to high current capabilities populate all three jumper shunts on J5 from VNEG to LGND.