SLVUCR7 September 2024 TPS26750
| Description | The 'Gaid' Task causes a warm restart of the PD Controller processor. |
|---|---|
| INPUT DATAX | None |
| OUTPUT DATAX | None |
| Task Completion | Technically this Task never completes because the processor restarts. However, because all HI registers return to their default AppConfig state upon reboot, all CMDx/DATAx registers will return to 0, which will mark this Task as complete. |
| Side Effects | The 'Gaid' Task causes a warm restart of the PD Controller processor. PD Controller can momentarily NAK I2C transactions while rebooting. |
| Additional Information | The PD controller is in the 'APP ' mode, then it immediately goes to the Error Recovery state then after delaying 1 second (typical) it does a warm restart. The register settings revert back to the original AppConfig configuration set by the user in the Application Customization Tool. |