SLVUCR7 September 2024 TPS26750
| Description | The 'SSrC' Task instructs the PD Controller to send a SourceCapabilities message at the first opportunity while maintaining policy enginecompliance. |
|---|---|
| INPUT DATAX | None |
| OUTPUT DATAX | Byte 1: Standard Task Return Code. See also Table 5-1. |
| Task Completion | The 'SSrC' Task completes either when the Sink Capabilities message GoodCRC is received or the Task otherwise fails. The 'SSrC' Task shall be considered rejected if:
|
| Side Effects | Other registers can change as a result of the contract negotiation that begins with the new Source Capabilities message. |
| Additional Information | None |