SLVUCD4 November 2022 DRA821U , DRA821U-Q1 , TPS6594-Q1
To achieve a system functional safety level of ASIL-B, the following PDN features are available:
The PDN has an in-line, external power FET, as shown in Figure 3-1, between the input supply and PMICs. The voltage before and after the FET is monitored by the PMIC, and the PMIC controls the FET through the OVPGDRV pin. The FET can quickly isolate the PMIC when an over-voltage event greater than 6 V is detected on the input supply to protect the system from being damaged. Any power connected upstream from the FET is not protected from over voltage events. In Figure 3-1 the load switches that supply power to the MCU and Main I/O domains, the discrete buck supplying the DDR, and the discrete LDO supplying EFUSE are all connected after the FET to extend the over voltage protection to these processor domains and discrete power resources.
The PMIC internal over voltage and under voltage monitoring and their respective monitoring threshold levels are enabled by default and can be updated through I2C after startup. PMIC power rails connected directly to the processor are monitored by default.
The steps for configuring and starting the watchdog can be found in the TPS6594-Q1 data sheet. Setting the DISABLE_WDOG signal high on GPIO_8 disables the watchdog timer if this feature needs to be suspended during initial development or is not required in the system. An example of re-purposing GPIO_8 is provided in Section 7.4.
GPIO_7 is configured as the MCU error signal monitor, but must be enabled though the ESM_MCU_EN register bit. MCU reset is supported through the connection between the primary PMIC nRSTOUT pin and the MCU_PORz of the processor. Lastly, there are two I2C ports between the TPS6594-Q1 and the processor. The first is used for all non-watchdog communication, such as voltage level control, and the second allows the watchdog monitoring to be on an independent communication channel.
There is an option to use the EN_DRV pin to indicate an error has been detected and the system is entering SAFE state. This signal can be utilized if the system has external circuitry that needs to be driven by an error event. In this PDN, the EN_DRV is not utilized, but available if needed.