SLVK304 April   2026 TMUX182-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single-Event Latch-up (SEL) Results
    2. 5.2 Single-Event Transients (SET) Results
  9. 6Summary
  10. 7References

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the MSU Cyclotron Radiation Effects Facility using a superconducting cyclotron and an advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For this study, ion flux of 1 × 105 ions/cm2-s were used to provide heavy-ion fluences of approximately 1 × 107 ions/cm2 for SEL testing. For the experiments conducted on this report, 109Ag ions at angle of incidence of 0° for an LETEFF of 47MeV × cm2/mg were used. The total kinetic energy of 109Ag in the vacuum is 2.125GeV (19.5 MeV/nucleon). Ion uniformity for these experiments was 91.88%.

Figure 4-1 shows one of the four TMUX182-SEP test boards used for experiments at the MSU facility. The in-air gap between the device and the ion beam port window was maintained at 50mm for all runs.

 TMUX182-SEP Evaluation Board at the MSU FacilityFigure 4-1 TMUX182-SEP Evaluation Board at the MSU Facility
 TMUX182-SEP Thermal Image for SELFigure 4-2 TMUX182-SEP Thermal Image for SEL