SLVK280 March 2026 INA1H182-SEP
The INA1H182-SEP was biased in a variety of different conditions for SEE testing at the recommended minimum and recommended maximum supply voltages. Midsupply or GND was used for REF. Current was monitored over time for both supplies VS+, VS- and the instrumentation amplifier inputs -IN and +IN.
Figure 4-3 shows an example of the INA1H182-SEP device mounted through a socket on a characterization board. During SEL qualification, the device was heated using forced hot air, maintaining an IC temperature at 125°C. During SEL testing, the devices were soldered into a coupon board, allowing direct airflow access to the heater. For SET testing, devices were mounted in a socket for the easy exchange of units.
Figure 4-3 Characterization Board