SLVK265 March 2026 TRF0108-SEP
The production TRF0108-SEP is rated to a total ionizing dose (TID) of 30krad(Si), with 50krad(Si) as information-only data. In the course of the SEE testing, the heavy-ion exposures delivered approximately 1krad(Si) per 106 ions/cm2 run. The cumulative TID exposure for each device respectively, over all runs each underwent, was determined to be greater than 30krad(Si). The production TRF0108-SEP devices used in the studies described in this report stayed within specification and were fully-functional after the heavy-ion SEE testing was completed.