SLVK228 October   2025 TPS7H1121-SEP

 

  1.   1
  2.   TPS7H1121-SEP Single-Event Effects (SEE)
  3.   Trademarks
  4. 1 Introduction
  5. 2 Single-Event Effects (SEE)
  6. 3 Device and Test Board Information
    1. 3.1 Device and Test Board Information Continued
  7. 4 Irradiation Facility and Setup
  8. 5 LETEFF and Range Calculation
  9. 6 Test Setup and Procedures
  10. 7 Destructive Single-Event Effects (DSEE)
    1. 7.1 Single-Event Latch-up (SEL) Results
    2. 7.2 Single-Event Burnout (SEB) and Single-Event Gate Rupture (SEGR) Results
  11. 8 Single-Event Transients (SET)
  12. 9 Event Rate Calculations
  13. 10Summary
  14.   A References

Single-Event Effects (SEE)

The primary concern for the TPS7H1121-SEP is the robustness against the destructive single-event effects (DSEE): single-event latch-up (SEL), single-event burnout (SEB), and single-event gate rupture (SEGR). In mixed technologies such as the BiCMOS process used on the TPS7H1121-SEP, the CMOS circuitry introduces a potential for SEL susceptibility.

SEL can occur if excess current injection caused by the passage of an energetic ion is high enough to trigger the formation of a parasitic cross-coupled PNP and NPN bipolar structure (formed between the p-sub and n-well and n+ and p+ contacts) [1,2]. The parasitic bipolar structure initiated by a single-event creates a high-conductance path (inducing a steady-state current that is typically orders-of-magnitude higher than the normal operating current) between power and ground that persists (is latched) until power is removed, the device is reset, or until the device is destroyed by the high-current state. The TPS7H1121-SEP was tested for SEL at the maximum recommended input voltage (VIN) of 14V. The output of the TPS7H1121-SEP was configured to the max (13.3V) and min (0.6V) voltages. The output load was configured depending on the output voltage. During the 13.3V testing a constant resistance value of 6.6Ω was used to create a 2A load on the output. During the 0.6V testing a load high enough to maintain a device temperature of 125°C was used. For the 9 devices tested under SEL conditions, the TPS7H1121-SEP did not exhibit any SEL with heavy-ions with LETEFF = 48 MeV·cm2/mg at flux 9.51 × 104 to 1.46 × 105 ions/cm2/s, fluence of ≈107 ions/cm2, and a die temperature of ≈ 125°C. To see more details on the SEL testing of the TPS7H1121-SEP, please refer to Section 7.1.

The TPS7H1121-SEP was evaluated for SEB/SEGR at a maximum input voltage of 14V in the enabled and disabled mode with the output voltage configured to be either 13.3V or 0.6V. For the 0.6V case, the load was set to a CR value of 6Ω for a load of 0.1A to prevent the device from heating ≳25°C, while for the 13.3V case, the load was set to 6.6Ω to get a load of 2A. Because the MOSFET has shown to be susceptibility to burnout decrement with temperature [5], the device was evaluated while operating under room temperatures, so no external thermal control device was used. During the SEB/SEGR testing, not a single current event was observed, demonstrating that the TPS7H1121-SEP is SEB/SEGR-free up to LETEFF = 48 MeV·cm2/mg at a flux of 8.78 × 104 to 1.60 × 105 ions/cm2/s, fluences of ≈107 ions/cm2, and a die temperature of ≈25°C. To see more details on the SEB/SEGR testing of the TPS7H1121-SEP, please refer to Section 7.2.

For SET testing, the TPS7H1121-SEP was characterized at a VIN of 5 and 12V. VOUT was configured to be 3.3V with a CR value of 3.3Ω for a load of 1A. During SET testing the VOUT, SS, and PG signals were monitored. During SET testing, not a single transient was observed, demonstrating that the TPS7H1121-SEP is SET/SEFI-free up to LETEFF = 48 MeV·cm2/mg at a flux of 1.02 × 105 to 1.31 × 105 ions/cm2/s, fluences of ≈107 ions/cm2, and a die temperature of ≈25°C. To see more details on the SET testing of the TPS7H1121-SEP, please refer to Section 8.