SLVA504A February   2012  – July 2021 DRV8143-Q1 , DRV8144-Q1 , DRV8145-Q1 , DRV8163-Q1 , DRV8242-Q1 , DRV8243-Q1 , DRV8244-Q1 , DRV8245-Q1 , DRV8263-Q1 , DRV8800 , DRV8801 , DRV8802 , DRV8803 , DRV8804 , DRV8805 , DRV8806 , DRV8811 , DRV8812 , DRV8813 , DRV8814 , DRV8818 , DRV8821 , DRV8823 , DRV8824 , DRV8825 , DRV8828 , DRV8829 , DRV8830 , DRV8832 , DRV8832-Q1 , DRV8833 , DRV8834 , DRV8835 , DRV8836 , DRV8837 , DRV8840 , DRV8841 , DRV8842 , DRV8843 , DRV8844 , DRV8870 , DRV8871 , DRV8872 , DRV8904-Q1 , DRV8906-Q1 , DRV8908-Q1 , DRV8910-Q1 , DRV8912-Q1

 

  1. 1Sources of Power Dissipation in an Integrated Driver
    1. 1.1 H-Bridge
      1. 1.1.1 H-Bridge Driver Using High-Side Recirculation
      2. 1.1.2 H-Bridge Driver Using Low-Side Recirculation
    2. 1.2 Half Bridge
      1. 1.2.1 Half Bridge Driver Using High-Side Recirculation
      2. 1.2.2 Half Bridge Driver Using Low-Side Recirculation
  2. 2Example Calculation
    1. 2.1 H-Bridge
      1. 2.1.1 High-Side Recirculation Example
      2. 2.1.2 Low-Side Recirculation Example
    2. 2.2 Half Bridge
      1. 2.2.1 Half-Bridge High-Side Recirculation Example
      2. 2.2.2 Half-Bridge Low-Side Recirculation Example
  3. 3References
  4. 4Revision History

Half Bridge Driver Using High-Side Recirculation

Figure 1-3 Half Bridge Driver Using High-Side Recirculation

The above figure shows the switching sequence of a half bridge in PWM regulation between Load - LS (region # 1) and Load - HS (region # 5) with other transitions (region # 2, 3, and 4 for rising edge and region # 6, 7, and 8 for falling edge). The load is assumed to be a high side load (connected directly to supply or through a external high side FET). The power dissipation on each FET is as follows:

Table 1-3 Power Dissipation for Half-Bridge with High-Side Recirculation
Region Time ratio within PWM cycle HS [W] LS [W]
1 D1 0 RON × IL2
2 VM/SRLSOFF x fPWM 0 0.5 x VM x IL
3 tDEAD_LSOFF x fPWM VD x IL 0
4 VD/SRHSON x fPWM 0.5 x VD x IL 0
5 (1 - D)1 RON × IL2 0
6 VD/SRHSOFF x fPWM 0.5 x VD x IL 0
7 tDEAD_LSON x fPWM VD x IL 0
8 VM/SRLSON x fPWM 0 0.5 x VM x IL
  1. If the slew time is significant portion of the PWM period, we recommend to adjust the duty cycle number based on slew times for regions # 1 and 5.

In Table 1-3,

  1. RON = FET on-resistance [ohm]
  2. fPWM = PWM switching frequency [Hz]
  3. VM = Supply voltage to the driver [V]
  4. IL = Load current [A]
  5. D = PWM duty cycle between 0 and 1
  6. SRLSOFF = Output voltage slew rate during rise when LS is turned off [V/sec]
  7. SRLSON = Output voltage slew rate during fall when LS is turned on [V/sec]
  8. VD = FET body diode forward bias voltage [V]
  9. tDEAD_LSOFF = dead time after LS has been turned off [sec]
  10. tDEAD_LSON = dead time before LS is turned on [sec]
  11. SRHSON = Output voltage slew rate during rise when HS is turned on [V/sec]
  12. SRHSOFF = Output voltage slew rate during fall when HS is turned off [V/sec]

If we assume power dissipation in regions #4 and #6 are negligible, slews rate match for rising and falling edges, dead times are equal, then power dissipation for each FET can be approximated as follows:

  1. PHS = [RON × IL2 x (1-D)] + [2 x VD x IL x tDEAD x fPWM]
  2. PLS = [RON × IL2 x D] + [VM x IL x (VM / SR) x fPWM]

Compared to a H-bridge driver, the power dissipation due to conduction losses is approximately cut in half, however, the switching losses remain the same.