SLUUDI8 March 2026 AM13E23019
The BSL_CONFIG_ID is a predetermined signature ID that identifies this as a Bootloader configuration structure. This 32-bit field serves as an identifier for the BSL configuration.
Usage: This field identifies the structure as a BSL configuration structure. It is a fixed value that should not be modified by users. The default value is 0x05000000.
Returned in Get Device Info: The BSL_CONFIG_ID is included in the response to the Get Device Info command (CMD_API_Get_Identity). This allows the host to identify the BSL configuration version or type.