SLUUCN4B January 2023 – December 2024
This command enables/disables Permanent Failure to help streamline production testing.
The initial setting is loaded from Mfg Status Init[PF_EN]. If the ManufacturingStatus()[PF_EN] = 0, sending this command enables Permanent Failure protections and the ManufacturingStatus()[PF_EN] = 1 and vice versa.
In UNSEALED mode, ManufacturingStatus()[PF_EN] status is copied to Mfg Status Init[PF_EN] when the command is received by the gauge. The BQ40Z50-R5 device remains on its PF enable/disable setting prior to a reset.