SLUAAF9 September 2021 UCC28782
Output voltage is detected by controller through VS pin, However, it is not recommended to probe VS pin directly as the noise introduced by probing could cause protection mis-triggering. Instead, AUX winding voltage can be used for identifying whether OVP happens. If the divided voltage on VS pin exceed OVP threshold for three consecutive pulses, OVP is triggered.
Figure 3-3 OVP Delay to Action
Figure 3-4 OVP Delay to Action (Zoom
In)
Figure 3-5 OVP ActionCH2: AUX winding voltage (Vaux), CH1: PWML, CH3: Output voltage.