SLUAAF9 September   2021 UCC28782

 

  1.   Trademarks
  2. 1 Initial Board Visual Inspection and Start-up Check
  3. 2 Typical System Operating Waveforms
    1. 2.1 SBP2 Mode
    2. 2.2 SBP1 Mode
    3. 2.3 LPM mode
    4. 2.4 LPM to ABM Mode Transition
    5. 2.5 ABM Mode
    6. 2.6 ABM to AAM Mode Transition
    7. 2.7 AAM Mode
  4. 3Typical System Protection Waveforms
    1. 3.1 Over-Power Protection (OPP)
    2. 3.2 Output Overvoltage Protection (OVP)
    3. 3.3 Output Short-Circuit Protection (SCP)
  5. 4Common Issues and Solutions
    1. 4.1 VDD Boost Converter Survival Mode
      1. 4.1.1 Survival Mode Due To Boost Inductor DCR Too High.
      2. 4.1.2 System Stays In Survival Mode When the Output Voltage is Low Such as 3.3V/5V/9V
    2. 4.2 10% Load Efficiency Might not Meet spec. in USB-PD Application, Especially at 5 V/9 V Output Condition
    3. 4.3 Transient
      1. 4.3.1 BIN/BSW Pin Damage During LPM to ABM Mode Transition
      2. 4.3.2 SR MOSFET VDS Overstress at Survival Mode
      3. 4.3.3 SR MOSFET Vds Voltage Overstress Due to PWMH Partial Turn On At Load Transition
  6. 5References

Initial Board Visual Inspection and Start-up Check

Before powering up the design board, the first step is to thoroughly review the design to make sure all design parameters are calculated properly. The Excel Design Calculator is a helpful tools to check the accuracy of the design. It is recommended to do a visual inspection to check for the following:

  • Solder bridges
  • Solder balls
  • Solder skips
  • Cold solder joints
  • Lifted pads

After visual inspection, the user can also use a multimeter to check the solder, Multimeter locked to diode location, Red probe connected to IC ground, Black probe connected to each pin. There should be a ~0.5 V-0.7 V voltage presents on the multimeter, if not, check solder of this pin. Figure 1-1 demonstrates probing UCC28782 Pins with a digital multimeter.

GUID-20210804-CA0I-SHBQ-S8DS-MDDNF8QGKGQN-low.jpgFigure 1-1 Probing UCC28782 Pins with a Digital Multimeter

When the solder inspection is complete, the board can input a low voltage, next steps are input short-circuit investigation / HV start circuits operation check / CS pin fault detection and input brown in voltage (startup voltage) detection:

  1. Step 1: Set input voltage source to Vin=5 Vrms while limiting its current to 0.5 A, measure the input current. After a brief low inrush peak current, there should be almost zero continuous input current, if an excessive current is observed, there may be a short or abnormally low impedance in the circuit.
  2. Step 2: If zero current is observed. Move to VDD pin to check if HV start circuits working properly, 25 Vrms voltage implied on the input, the captured waveform of VDD as shown in Figure 1-2: If VDD voltage can be charged to ~17.5 V, it indicates the HV start circuits working normal. if not please refer to Debugging UCC28780 ACF Converter Start-up Issues section 7.3, Start-up Failure Due to VDD Clamped Low.
    GUID-35FE7F78-3501-40C8-99C4-EE5E22B54EE9-low.png Figure 1-2 VDD Start Up and Hiccup at Below Brown In Voltage
  3. Step 3: Zoom in waveform at the point when VDD reaches to its turn on threshold (17.5 V), capture low side driver signal PWML, if only one pulse with a width of 2us is observed, see Figure 1-4, this is the correct behavior at the input voltage which lower than start up voltage. Please refer to Debugging UCC28780 ACF Converter Start-up Issues section 6.1 Observation of Zero or Only One PWML Pulse.
    GUID-20210804-CA0I-7HN8-L9MJ-BCZ7KBGDQRDX-low.png Figure 1-3 VDD Restart
    GUID-20210804-CA0I-ZFFQ-9LZZ-X7L4SVFW3NZL-low.png Figure 1-4 CS Pin Fault Detection - Only 1 Pulse With 2us Width
  4. Step 4: Gradually increase input voltage until the user can see four consecutive pulses shown in Figure 1-5. The first pulse is for CS pin fault detection, the second, third, fourth pulses are for brown in voltage detection. When the AC input voltage is lower than brown in voltage. The user will always see four pulses at each VDD restart cycle. Further increasing the input voltage until it is above the brown in voltage, the board should be powered up if there is no protection occurring.
    GUID-20210804-CA0I-HQ0P-MV85-RTPTN5ZCNFKB-low.png Figure 1-5 Brown-in Voltage Detection – 4 Consecutive Pulses