SLDU028A January   2018  – March 2020

 

  1.   TPS65313-EVM User’s Guide
    1.     Trademarks
    2. TPS65313-EVM Top View With Basic External Connections
    3. TPS65313-EVM Input, Output Voltages, and Load Current Requirements
    4. TPS65313-EVM Jumper Settings
    5. TPS65313-EVM GUI Installing and Opening the GUI
    6. TPS65313-EVM Power-Up and Power-Down Procedure
    7. TPS65313 GUI
      1. 6.1 Device Controls Page
        1. 6.1.1 Re-Initialize USB2ANY Button
        2. 6.1.2 WAKE Button
        3. 6.1.3 Power Off Button
        4. 6.1.4 Device Status Update
        5. 6.1.5 State Transitions
        6. 6.1.6 Enable Q&A Watchdog
        7. 6.1.7 MCU Error Signal Monitor (ESM)
        8. 6.1.8 SPI Status Bits
        9. 6.1.9 Moniter ENDRV and NRES Button
      2. 6.2 Register Map Page
      3. 6.3 EEPROM Programming Page
    8. TPS65313-EVM Typical Plots
      1. 7.1 Efficiency Plots
      2. 7.2 Power-Up Plots
      3. 7.3 Power-Down Plots
      4. 7.4 Ripple Voltage Plots
      5. 7.5 Load Transient Plots
      6. 7.6 Stability Measurements
    9. TPS65313-EVM Schematic Diagram
    10. TPS65313-EVM Part List
    11. 10 PCB Layer Diagram
    12. 11 Description of the Watchdog Algorithm Implemented on EVM
  2.   Revision History

TPS65313-EVM GUI Installing and Opening the GUI

This section provides the step-by-step instructions to install the TPS65313-EVM GUI on a computer.

  1. Unzip the TPS65313GUI.zip file and double click on the Setup_TPS65313_EVM.exe executable file.
  2. Figure 2 shows the GUI installer window in a sequence (1, 2, 3, and 4). When the installer window opens, click the Next button. Select the I accept the agreement radio button and then click the Next button.
  3. tps65313-evm-gui-installation-sequence.gifFigure 2. TPS65313-EVM GUI Installation Sequence
  4. In the next window select the LabVIEW RTE checkbox if it is not installed already on the computer. The user must have LabVIEW 2014 runtime. Make sure the computer is connected to the internet because free online registration may be required.
  5. tps65313-evm-gui-labview-rte-installation-selection.gifFigure 3. TPS65313-EVM GUI LabVIEW RTE Installation Selection
  6. After the LabVIEW RTE is installed, click the Next button to install the EVM GUI. Click the Finish button to complete the installation.
  7. When installation is complete, click the Windows Start button and select All Programs. Navigate to the Texas Instruments folder and click TPS65313-EVM to open the GUI.