SLAU821 October 2019
Figure 7 shows the options for connecting the CAPTIVATE-EMC to a host computer:
Open CapTIvate Design Center on the host computer.
Figure 7. Connection to CapTIvate Design Center Open the FR2676_CAPTIVATE-EMC example project in CapTIvate Design Center. Select Communications → Connect from the menu bar in CapTIvate Design Center to enable target communications. When the user touches a button, the button status is reflected in CapTIvate Design Center (see Figure 8).
Figure 8. CAPTIVATE-EMC Project Canvas