SLAA898 September 2022 TAS3251 , TPA3255
When comparing the integrated Class-D implementation to the discrete implementation, there are multiple advantages to consider. The first, and most evident advantage when observing Figure 1-1 and Figure 1-2, is the simplification of the circuit design. By using an integrated Class-D amplifier with digital input, it can receive the signal input directly from a microcontroller. Thus, the integrated Class-D amplifier, in this case, removes the need for signal conditioning circuitry. Second, because the integrated Class-D amplifier simplifies the circuit by replacing multiple components, it reduces the overall bill of material (BOM) cost. By choosing representative parts for each block replaced by the integrated Class-D amplifier, the estimated 1-kU cost of the replaced components is approximately double that of the integrated Class-D amplifier. This evaluation also includes the necessary external passive components for the implementation of the Class-D amplifier. Third, implementing a power amplifier using the integrated Class-D amplifier over the discrete implementation introduces board-size savings. Doing a layout analysis of the discrete components replaced by the integrated Class-D amplifier shows that they occupy approximately eight square inches (not including heat sinks) in total. The integrated Class-D amplifier, specifically the TAS3251 device for this analysis, requires only approximately three square inches. The size savings offered by the integrated Class-D amplifier can help greatly reduce system size. Finally, TI’s Class-D amplifiers offer high performance, and further functionality improvements, over the typical discrete implementation. The TAS3251 device has integrated protection and error reporting on-chip that enables real-time monitoring for overvoltage, undervoltage, and clipping, while also protecting against events like short circuits. Additionally, the TAS3251 device has greater than 108 dB SNR, and less that 0.01% total harmonic distortion (THD), so it delivers strong audio performance at the output of the amplifier.