SLAA898 September 2022 TAS3251 , TPA3255
Figure 1-1 shows a traditional, discrete implementation for the power amplifier in a fire safety application.
This implementation scheme requires many different components to achieve the waveform amplification. The transceiver at the beginning of the signal chain enables communication between the power amplifier board and a central control unit. The digital processing block then decides which audio signal to send through the system. Then, the audio CODEC, along with various operation amplifiers, switches, and a triangle-wave generator, condition the audio signal to be a usable input for the FET driver. The FET driver then drives the FETs, which creates the final audio signal. That signal is then sent through the transformer and to the notification appliance circuits (NACs).
This implementation scheme requires many different components to achieve the waveform amplification. The transceiver at the beginning of the signal chain enables communication between the power amplifier board and a central control unit. The digital processing block then uses the appropriate audio signal to send through the system. Then, the audio CODEC, along with various operation amplifiers, switches, and a triangle wave generator, condition the audio signal to be a usable input for the FET driver. The FET driver then drives the FETs, creating the final audio signal. That signal is then sent through the transformer and to the NACs.