SLAA898 September 2022 TAS3251 , TPA3255
Unless choosing a transformer that covers a wide range of audio frequencies, pay attention to the power limit. For instance, if 100 W is to be delivered to different speakers, a greater than 100-W transformer should be applied. Also, it is best not to use the full power of the transformer, because at the power limit, the current in the transformer is high and near the saturation of the transformer. As a result, the turns ratio (from the primary to secondary side) can be much lower, and equivalent resistance on the primary side is much lower, which leads to lower efficiency for the Class-D amplifier.