SLAA475A October 2010 – March 2019 MSP430L092
The errors themselves have different dependencies, such as the reference voltage or the A-Pool clock.
The overdrive error is dependent on the A-Pool clock frequency. A high frequency increases the possibility that an overdrive error occurs. With the highest clock frequency, the maximum error is 1 voltage step.
The internal reference is refreshed on a regular time base. Between the refresh cycles, the reference can have a slight drift, which can have an impact on the measurement. The update frequency of the reference is selected to meet the specification limits shown in the data sheet.
Depending on the input divider for the signal, the resolution of the signal is limited. The accuracy changes with divider settings. Table 3 shows these dependencies.
| Divider Setting | Maximum Accuracy of Input Signal |
|---|---|
| 1 | 1 mV |
| 2 | 2 mV |
| 4 | 4 mV |