SLAA202B February 2005 – December 2018 MSP430F149 , MSP430F149 , MSP430F2252-Q1 , MSP430F2252-Q1 , MSP430F2272-Q1 , MSP430F2272-Q1 , MSP430F2274 , MSP430F2274 , MSP430FG4619 , MSP430FG4619
These services are in charge of starting an IrLAP discovery procedure when requested by the user layer. Its only involvement is in adding the service hints and the device information field to the IrLAP XID frame. As shown in Figure 8, the XID response frame includes a field for the device information named discovery info. This field, as described by the IrLMP documentation, is composed of the service hints and the device nickname. The device nickname is itself divided into two other fields which are the character set and the actual name of the device as shown in Figure 12. The service hints provided in this application are 08204h. As can be seen from Table 1, these bits correspond to an extension bit, PDA/Palmtop support, and IrCOMM implementation. The total length of the device information field must not exceed 23 bytes, although the IrLAP XID frame reserves 32 bytes.
Figure 12. Device Information Field Format