SLAA202B February 2005 – December 2018 MSP430F149 , MSP430F149 , MSP430F2252-Q1 , MSP430F2252-Q1 , MSP430F2272-Q1 , MSP430F2272-Q1 , MSP430F2274 , MSP430F2274 , MSP430FG4619 , MSP430FG4619
After the frame has been identified as an IrLAP I-frame carrying user-data, the first test in the IrLMP parsing process is to determine if it is an IrLMP frame carrying data, IrLMP-connection parameters, or TTP-connection parameters. After bit 7 of the third IrLAP byte has been tested and if it is a 0, then the frame is positively identified as an IrLMP frame carrying data. Figure 13 shows the encoding of an IrLMP data frame.
Figure 13. IrLMP Data Transfer Frame Format