SBOU278 December   2021

 

  1.   Trademarks
  2. 1Overview
    1. 1.1 OPT4001YMNEVM Kit Contents
    2. 1.2 Related Documentation from Texas Instruments
  3. 2OPT4001YMNEVM Hardware
    1. 2.1 Theory of Operation for the OPT4001YMNEVM
    2. 2.2 OPT4001YMNEVM Hardware Overview
  4. 3OPT4001YMNEVM Software
    1. 3.1 Hardware Requirements
    2. 3.2 Software Installation
    3. 3.3 Typical OPT4001YMNEVM Hardware Setup
    4. 3.4 Launching the OPT4001EVM Software
    5. 3.5 OPT4001EVM Software Operation
      1. 3.5.1 Getting Started
      2. 3.5.2 Feature Descriptions
  5. 4Schematic, PCB Layout, and Bill of Materials
    1. 4.1 Flex Coupon Board
      1. 4.1.1 Schematic
      2. 4.1.2 PCB Layout
      3. 4.1.3 Bill of Materials
    2. 4.2 Rigid Coupon Board
      1. 4.2.1 Schematic
      2. 4.2.2 PCB Layout
      3. 4.2.3 Bill of Materials
    3. 4.3 Motherboard
      1. 4.3.1 Schematic
      2. 4.3.2 PCB Layout
      3. 4.3.3 Bill of Materials
  6. 5Troubleshooting
    1. 5.1 Microsoft Windows 7 Manual Driver Installation

Getting Started

To quickly start using the device, click the Operation Select drop-down menu and select Continuous to bring the device out of power down mode. Then click Start Capture to begin data capture. The green LED on the motherboard will turn off. Lux data will appear above the lux plot as shown. The plot will also start to populate with the device lux readings.

GUID-20211221-SS0I-JWBM-JZGG-GZHZTDFVFMDS-low.png Figure 3-13 GUI Capture Running

If the GUI is not responsive, check the other Latte scripts window, which is minimized by default. If the message Operation I2C Register Read for command [REGRx01] Failed is displayed this means that the OPT4001 IC or coupon is not detected by the motherboard. Ensure the coupon is plugged in and properly oriented.