SBOU278 December   2021

 

  1.   Trademarks
  2. 1Overview
    1. 1.1 OPT4001YMNEVM Kit Contents
    2. 1.2 Related Documentation from Texas Instruments
  3. 2OPT4001YMNEVM Hardware
    1. 2.1 Theory of Operation for the OPT4001YMNEVM
    2. 2.2 OPT4001YMNEVM Hardware Overview
  4. 3OPT4001YMNEVM Software
    1. 3.1 Hardware Requirements
    2. 3.2 Software Installation
    3. 3.3 Typical OPT4001YMNEVM Hardware Setup
    4. 3.4 Launching the OPT4001EVM Software
    5. 3.5 OPT4001EVM Software Operation
      1. 3.5.1 Getting Started
      2. 3.5.2 Feature Descriptions
  5. 4Schematic, PCB Layout, and Bill of Materials
    1. 4.1 Flex Coupon Board
      1. 4.1.1 Schematic
      2. 4.1.2 PCB Layout
      3. 4.1.3 Bill of Materials
    2. 4.2 Rigid Coupon Board
      1. 4.2.1 Schematic
      2. 4.2.2 PCB Layout
      3. 4.2.3 Bill of Materials
    3. 4.3 Motherboard
      1. 4.3.1 Schematic
      2. 4.3.2 PCB Layout
      3. 4.3.3 Bill of Materials
  6. 5Troubleshooting
    1. 5.1 Microsoft Windows 7 Manual Driver Installation

Microsoft Windows 7 Manual Driver Installation

This section outlines the manual driver installation process. If you are using Windows 7 or if the Windows device manager shows 2 USB Serial Devices under other devices as shown in Figure 5-1 when the EVM is plugged in instead of COM ports, please use the following steps to correctly install the USB drivers. If two USB Serial Device devices show up as COM ports automatically (as is the case with Windows 10), then this section can be skipped.

GUID-62FE4B89-9894-4D6B-8ADE-D1088489E27F-low.pngFigure 5-1 OPT4001YMNEVM on Microsoft®Windows® 7 With Drivers not Installed
  1. Open the device manager.
    GUID-D4F06134-96D8-4E11-9BB8-8A61A7EEDA85-low.png
  2. Right click on USB Serial Device and select Properties.
  3. Click the Update Driver… button.
    GUID-EC06EDA6-39B0-4D0B-B373-FFF94C5F16D1-low.png
  4. Click Browse my computer for driver software
    GUID-4804D624-2FA9-4E1A-B5DD-068225B51905-low.jpg
  5. Click Let me pick from a list of device drivers on my computer.
    GUID-EC594B67-5CA0-42DF-BC6D-145DAAE21074-low.png
  6. Select Show All Devices and click the Next button.
    GUID-43A50BF9-4833-496D-B6B8-CC52F12ABCDE-low.png
  7. Click the Have Disk… button.
    GUID-DFF0BB90-797A-44AF-BFDC-F420543A767A-low.png
  8. Click the Browse… button.
    GUID-E42F22AE-F090-4329-8D35-1910F9B8088B-low.png
  9. Navigate to “C:\Users\<username>\Documents\Texas Instruments\Latte\projects\OPT4001\drivers” and choose MSP430_CDC. Click the Open button.
    GUID-4C1717B4-9663-4CEB-A85E-FAFD92253355-low.jpg
  10. Click the OK button
    GUID-DD84CB04-77EC-4E0E-9290-516905C8EDB5-low.png
  11. Select the first USB serial device and click the Next button.
    GUID-524AA029-CE1D-4C7D-9DBD-376C755B32B9-low.jpg
  12. Click the Yes button.
    GUID-A4CE1766-746C-4235-91C0-9BE48CE4514D-low.png
  13. The driver should now install properly.
    GUID-996D1D0B-8104-4831-967B-6FD1EAE68775-low.jpg
  14. Now repeat this process (steps 1 to 13) for the second USB Serial Device. All steps are the same except for step 2 and step 11. In step 2 make sure to right click the second USB Serial Device. Likewise, on step 11 make sure to select the second USB Serial Device when installing the driver as the following figure shows.
    GUID-41F12D34-EF47-4FC9-AB4F-5A3AF61C1272-low.jpg
  15. When the driver is installed, you will see the following message.
    GUID-EE7CC113-9015-4349-89C7-C855168B7A83-low.jpg
  16. The two USB Serial Device devices should now appear in the device manager under Ports (COM & LPT) as the following image shows.
GUID-20211220-SS0I-FRDV-V74T-1LQDFL11V5ZJ-low.png